It's also possible to iterate over all the features offered by a device or a subtree of this. To see how this is done refer to the description of the class mvIMPACT.acquire.Component.
To access e.g. the device information related features, the locator instance must be initialised in a different way:
pDev = getTheDevicePointerFromSomewhere()
locator = acquire.DeviceComponentLocator (pDev, dltInfo, "DeviceInformation")
deviceVersion = acquire.PropertyS()
locator.bindComponent(deviceVersion, "DeviceVersion")
# now the property is ready to use when available:
if deviceVersion.isValid:
print deviceVersion.name() + ": " + deviceVersion.read()
else:
# oops... The feature is not offered by this device