Impact Acquire SDK .NET
Loading...
Searching...
No Matches
GenICam Interface Layout (File Stream)

Classes and functions that will be available if the device is used with the GenICam interface layout. More...

Collaboration diagram for GenICam Interface Layout (File Stream):

Classes

class  DevFileStream
 A helper class derived from System.IO.Stream used to read from and write to a file on a device. More...

Detailed Description

Classes and functions that will be available if the device is used with the GenICam interface layout.

This group contains classes and functions that will be available if the device is used with the mv.impact.acquire.TDeviceInterfaceLayout.dilGenICam interface layout.