Impact Acquire SDK Java
Loading...
Searching...
No Matches
Which Shipped File Is Affected By Which License

This section lists files that are affected by one or more of the Used Third Party Software packages mentioned above.

Note
  • Files not listed here are not affected by any of the third party licenses.
  • When a certain license is listed for some platforms only, the file only makes use of the third party software on these platforms. E.g. A Windows® specific third party package cannot and therefore won't be used on Linux.
  • When a certain platform is not listed for a certain license, the library, application or file is either not shipped for this platform or does not make use of the third party software.

Runtime

This section lists files belonging to the runtime of Impact Acquire. A subset (or all) of these files need to be shipped by client applications using the Impact Acquire SDK!

Note
In following sections, a file named XYZ-lib refers to
  • a file XYZ.dll on Windows®
  • a file libXYZ.so on Linux

BVS_CA-BN.H-lib / BVS_CA-BN.S-lib

PlatformRelevant Licenses
Windows
Linux

mvBlueFOX-lib

PlatformRelevant Licenses
Windows
Linux x86_64
Linux ARMhf/ARM64

mvDeviceManager-lib

PlatformRelevant Licenses
Windows
Linux x86_64
Linux ARMhf/ARM64

mvDisplay-lib

PlatformRelevant Licenses
Windows

mvGenTLConsumer-lib

PlatformRelevant Licenses
Windows
Linux x86_64
Linux ARMhf/ARM64

mvGenTLProducer-lib

PlatformRelevant Licenses
Windows
Linux

mvGenTLProducer.PCIe-lib

PlatformRelevant Licenses
Windows
Linux

mvImageProcessing-lib

PlatformRelevant Licenses
Windows
Linux x86_64

mvmDNSInterfaceResolver-lib

PlatformRelevant Licenses
Linux x86_64/ARMhf/ARM64

mvPropHandling-lib

PlatformRelevant Licenses
Windows
Linux

mvVirtualDevice-lib

PlatformRelevant Licenses
Windows
Linux x86_64
Linux ARMhf/ARM64

Applications

This section lists files coming as part of the Impact Acquire SDK but usually are not needed by client applications.

ContinuousCaptureFFmpeg

Building this example application is only possible using FFmpeg therefore the corresponding license applies.

DeviceConfigure

PlatformRelevant Licenses
Windows
Linux

IPConfigure

PlatformRelevant Licenses
Windows
Linux

GigEConfigure

PlatformRelevant Licenses
Windows

SmartFrameRecall.CS

Windows

ImpactControlCenter

PlatformRelevant Licenses
Windows
Linux