Impact Acquire SDK Java
Loading...
Searching...
No Matches
Iterate Over A Tree Of Features

It's also possible to iterate over all the features offered by a device or a subtree of this. To see how this is done refer to the description of the class mvIMPACT.acquire.Component.

To access e.g. the device information related features, the locator instance must be initialised in a different way:

Device pDev = getTheDevicePointerFromSomewhere();
DeviceComponentLocator locator = new DeviceComponentLocator(pDev, dltInfo, "DeviceInformation");
PropertyS deviceVersion = new PropertyS();
locator.bindComponent( deviceVersion, "DeviceVersion" );
// now the property is ready to use when available:
if( deviceVersion.isValid() )
{
System.out.println( String.format( "%s: %s", deviceVersion.name(), deviceVersion.read() ) );
}
else
{
// oops... The feature is not offered by this device
}