Impact Acquire SDK C++
Loading...
Searching...
No Matches
The 'Untrusted publisher' Dialog Box Appears When Installing A Driver On Windows® 7 Or Windows® Server 2008 R2

Symptoms

Please see here: https://support.microsoft.com/en-us/kb/2921916

Cause

Since Impact Acquire 2.15.2 files will be signed using a SHA256 certificate as required/recommended by Microsoft since 01.01.2016. Windows® versions smaller than Windows® 8 however do not fully support SHA256 certificates so some hotfixes are needed.

Resolution

Install the following Windows® patches(in THIS order):

  • KB3033929
  • KB2921916