Impact Acquire SDK C++
Loading...
Searching...
No Matches
Optimization Of Network Parameters

To improve performance, some system parameters may have to be adapted on the target system. For some of them, you may need to have administrator privileges.

  • An MTU of 9000 (at least 8000 should be used)
  • Via sysctl, some more optimizations could be made:
    sudo sysctl -w kern.ipc.maxsockbuf=8388608 // or more if possible
    sudo sysctl -w net.inet.udp.maxdgram=9216
    sudo sysctl -w net.inet.raw.recvspace=16777216 // or more if possible
    sudo sysctl -w net.inet.udp.recvspace=7454720 // or more if possible
    Note
    These changes are only valid for the running session and have to be set after each start of the system