Impact Acquire SDK C
Toggle main menu visibility
Loading...
Searching...
No Matches
General Issues
A Balluff Device Such As A BVS CA-G* (mvBlueCOUGAR-X) Or BVS CA-SF (mvBlueFOX3) Is Detected As A 3rd Party GigE Vision™/USB3 Vision™ Device Only
A GenICam™ Device Supporting The 'ValidValueSet' Node Inside Its XML File Cannot Be Initialised
A GenICam™ Device With A Floating Enum Entry Node Inside Its XML File Cannot Be Initialised
A Setting Of A GenICam™ Device Cannot Be Loaded Or Not All Features That Are Part Of The Setting Are Actually Applied To The Device
Calling 'imageRequestWaitFor' Never Returns / An Application No Longer Terminates After Upgrading To Impact Acquire 2.32.0 Or Greater
Checking For Updates No Longer Detects Updates
Random 'bad_alloc' Exceptions When Running With Active Image Processing Filters
The Presence Of A 3rd Party GenTL Producer Results In Impact Acquire To Crash
The Presence Of Another 3rd Party GenTL Producer Framework Results In Devices Not Being Detected By Both Frameworks
Applications That Need A Lot Of Thread Local Storage (TLS) Crash With Impact Acquire 3.6.3 Or Earlier
Known Issues
Generated on
3.8.1