Balluff - BVS CA-SF Technical Documentation
Loading...
Searching...
No Matches
Unattended Setups

Sometimes user interaction during an installation is not desired. This is where unattended setups come in. Using the original installation package this can be achieved like this:

./ImageAcquire-<platform>-<version>.sh -u

To control which components will get installed during this unattended session additional parameters can be passed to the script as described in the Installation Options chapter.

For a complete list of options type

./ImageAcquire-<platform>-<version>.sh -h

in a command shell and hit the ENTER key.