Balluff - mvVirtualDevice Technical Documentation
System Requirements

The mvVirtualDevice device package can be used to evaluate Impact Acquire functions and even implement the hardware specific part without having the Balluff imaging hardware installed yet.

For this reason the following components are recommended:

ComponentRecommendation
ProcessorPreferably multi core Intel or ARM CPUs
RAM4 GB in 32-bit OS; 8 GB in 64-bit OS
MainboardUSB connectors

Supported Operating Systems

Windows®

The following versions of Windows® are supported officially:

  • Microsoft Windows® 10 (64-bit)
  • Microsoft Windows® 11

Other Windows® versions might work as well but will not be tested on a regular basis. A complete list of supported Windows® versions can be found here.

Linux

The latest version for the required target platform of the Impact Acquire framework can always be found here: https://www.balluff.com/en-de/products/MP18308637.

Currently supported Kernel versions are:

  • Kernel 3.5.x or greater

macOS

The latest version for the required target platform of the Impact Acquire framework can always be found here: https://www.balluff.com/en-de/products/MP18308637.

Currently, macOS version 12 (Monterey) is supported.