Balluff - BVS CA-MLC / BVS CA-IGC / mvBlueFOX Technical Documentation
Using VLC Media Player

With the DirectShow Interface Impact Acquire compliant devices become video capture devices for the VLC Media Player.

Figure 1: VLC Media Player with a connected device via DirectShow

System Requirements

It is necessary that the following drivers and programs are installed on the host device (laptop or PC):

  • Windows 7 or higher, 32-bit or 64-bit
  • up-do-date VLC Media Player, 32-bit or 64-bit (here: version 2.0.6)
  • up-do-date Impact Acquire driver, 32-bit or 64-bit (here: version 2.5.6)
Note
Using Windows 10 or Windows 7: VLC Media Player with versions 2.2.0 have been tested successfully with older versions of Impact Acquire. Since version 3.0.0 of VLC Impact Acquire will be needed to work with devices through the DirectShow interface!

Installing VLC Media Player

  1. Download a suitable version of the VLC Media Player from the VLC Media Player website mentioned below.
  2. Run the setup.
  3. Follow the installation process and use the default settings.

A restart of the system is not required.

See also
http://www.videolan.org/

Setting Up A Device For DirectShow

For using devices, DirectShow needs a public driver that must be registered with the operating system. As described in Registering Devices , this can be done with the help of DeviceConfigure .

Note
If running a 64-bit DirectShow application, make sure to use a 64-bit version of DirectShow_Acquire, which can only be installed with a 64-bit version of DeviceConfigure . (And respectively for a 32-bit version)
  1. Connect the device to the host.
  2. Power the camera using a power supply at the power connector.
  3. Wait until the status LED turns blue.
  4. Open the tool DeviceConfigure ,
  5. set a friendly name ,
  6. and register the device for DirectShow .
Note
In some cases it could be necessary to repeat step 5.

Working With VLC Media Player

  1. Start VLC Media Player.
  2. Click on "Media -> Open Capture Device..." .

    Figure 2: Open Capture Device...

  3. Select the tab "Device Selection" .
  4. In the section "Video device name" , select the friendly name of the device:
    Figure 3: Video device name

  5. Finally, click on "Play" .
    After a short delay you will see the live image of the camera.

Changing Camera Properties

When selecting a DirectShow_Acquire camera as a DirectShow capture device (in the "Open Capture Device" dialog), there are two posibilities to display the camera property dialog:

A. Click the checkbox "Show more options" and append " :dshow-config" to the options in the bottom edit box:

Figure 1: Entering additional options for displaying the DirectShow_Acquire property dialog

B. Alternatively, press the button "Advanced options" and, in the window that is going to be displayed, click the checkbox "Device properties" followed by pressing "OK". This fills in all the relevant settings of the dialog into the edit box in the "Open Media : Capture Device" dialog from solution A above.

Figure 2: Advanced options dialog invokrd by the Media/Open Capture dialog

After selecting the activity to invoke (Play/Stream/Enqueue/Convert), the DirectShow_Acquire property dialog will open.

Figure 3: The property dialog for the DirectShow_Acquire capture device
Note
Most properties in this dialog control the camera directly, so they stay the same as long as the camera is not reset. Properties that control streaming (like the ImageDestination::PixelFormat) are set by the VLC Media Player each time the capture device is started.

After pressing "OK", the selected activity will start.

See also
If there are wrong colors in the resulting images, refer to Wrong Colors in the VLC Media Player .

Possibly there will be an error box like the one shown below, but you can safely ignore it by pressing "No" or "Cancel".

Figure 4: Error message during startup of capture property dialog