|
Balluff - BVS CA-MLC / BVS CA-IGC / mvBlueFOX Technical Documentation
|
0. WaitDigin DigIn0->On 1. WaitClocks <delay time> 2. TriggerSet 0 3. WaitClocks <trigger pulse width> 4. TriggerReset 5. Jump 0 <trigger pulse width> should not less than 100us.
As soon as digital input 0 changes from high to low (0), the HRTC waits the < delay time > (1) and starts the image expose. The expose time is used from the expose setting of the camera. Step (5) jumps back to the beginning to be able to wait for the next incoming signal.
WaitDigIn[On,Ignore] WaitDigIn[Off,Ignore]the minimum pulse width which can be detected by HRTC has to be at least 5 us.