Impact Acquire SDK C++
General Issues
Calling 'imageRequestWaitFor' Never Returns / An Application No Longer Terminates After Upgrading To Impact Acquire 2.32.0 Or Greater
Random 'bad_alloc' Exceptions When Running With Active Image Processing Filters
A GenICam Device Supporting The 'ValidValueSet' Node Inside Its XML File Cannot Be Initialised
A GenICam Device With A Floating Enum Entry Node Inside Its XML File Cannot Be Initialised
A Setting Of A GenICam Device Cannot Be Loaded Or Not All Features That Are Part Of The Setting Are Actually Applied To The Device
a Balluff device Such As A mvBlueCOUGAR-X Or mvBlueFOX3 Is Detected As A 3rd Party GigE/USB3 Vision Device Only
The Presence Of A 3rd Party GenTL Producer Results In Impact Acquire To Crash
Runtime Requirements
Generated on Mon Oct 9 2023 22:13:49