|
Impact Acquire SDK C++
|
ExposureTime or the BalanceRatio seem to miss in the feature tree displayed in ImpactControlCenterFirmwareVersion property contains Unknown getUserData related API accessible through the Device object is not availableFirmwareUpdater API is not possibleThe reason for this behaviour is an inconsistency in older version of the mvGenTLConsumer-lib that fails to detect devices with certain MAC addresses correctly.
The following table shows general compatibility issues for GigE Vision™ devices:
| Impact Acquire version | Potential detection issues |
|---|---|
| < 2.31.0 (Mar 07 2019) | Only devices using a MAC address from the following ranges are detected correctly: 0c:8d:50:80:00 - 0c:8d:61:7F:FF 0c:8d:63:00:00 - 0c:8d:63:7F:FF 0c:8d:70:80:00 - 0c:8d:70:BF:FF |
| 2.31.0 - 2.47.0 (Jul 28 2022) | Only when using customized devices using non Balluff MAC addresses AND custom product identifiers |
| > 2.47.0 | No |
The following table shows general compatibility issues for USB3 Vision™ devices:
| Impact Acquire version | Potential detection issues |
|---|---|
| <= 2.47.0 (Jul 28 2022) | Only when using customized devices using non Balluff vendor names |
| > 2.47.0 | No |
Use a compatible combination of device and Impact Acquire.