Balluff - BVS CA-GW Technical Documentation
Loading...
Searching...
No Matches
Connecting The Camera

To start the device please accomplish following steps:

  1. Connect the BVS CA-GW with a
    • suitable cable to a network (e.g. a switch) or PC directly
  2. Power the BVS CA-GW via power supply.
    The device will boot immediately.

After energizing BVS CA-GW via power supply the camera will start to boot.

Depending on the configuration of the network or the BVS CA-GW (more precisely: if DHCP is used or not), following IP addresses are assigned:

  • If the BVS CA-GW is configured to use a static IP address, the BVS CA-GW will use this one. In this case, the BVS CA-GW will only be accessible, if the IP address is valid for the current network.
  • With DHCP, the BVS CA-GW will get an IP address from the DHCP server (default setting).
  • Without DHCP, the BVS CA-GW will start with a logical link address (LLA) / zero configuration class B IP address ("169.254.X.X", netmask 255.255.0.0).
Note
Please have a look at LLA in the Glossary when using Linux and LLA.
Attention
"Network misconfiguration"

The camera will not be reachable if you are using a wrong static IP address.

→ Please be sure that that the IP address
  • does exist
  • is not used by anyone else in the same network
  • is a valid one
Note
If you have two NICs in your PC, please be sure that they are using different subnets, otherwise the system does not know which Ethernet interface is used to exchange the data.
Working example:

 192.168.0.1: PC Port1
 172.16.1.1:  PC Port2
 192.168.0.3: Cam1
 172.16.1.4:  Cam2

You can change settings like the static IP address to your needs (please have a look at: IPConfigure).

Further the BVS CA-GW starts the GigE Vision control server making the device actually discoverable using standard GigE Vision mechanism.

Boot sequence of BVS CA-GW