Balluff - BVS CA-GW Technical Documentation
Loading...
Searching...
No Matches
Recording sequences with pre-trigger

Introduction

With pre-trigger it is possible to record frames before and after a trigger event.

How it works

To use this functionality you have to set the mv Acquisition Memory Mode to "mvPretrigger". This can be used to define the number of frames which will be recorded before the trigger event occurs:

Figure 1: ImpactControlCenter - setting pre-trigger

Afterwards, you have to define the "AcquisitionStart" or "AcquisitionActive" event. In figure 1 this is Line4 as trigger event, which starts the regular camera streaming.

Now, start the camera by pressing "Live" and generate the acquisition event.

The camera will output the number of pre-trigger frames as fast as possible followed by the frames in live mode as fast as possible until the frame rate is in sync:

Figure 2: ImpactControlCenter - recorded / output images