Balluff - BVS CA-GW Technical Documentation
Loading...
Searching...
No Matches
Working with Event Control

Balluff/MATRIX VISION devices can generate Event notifications. An Event is a message that is sent to the host application to notify it of the occurrence of an internal event. With "Setting → Base → Camera → GenICam → Event Control" you can handle these notifications.

At the moment, it is possible to handle

  • Exposure End (= sensor's exposure end)
  • Line 4 (= DigIn0) Rising Edge
  • Line 5 (= DigIn1) Rising Edge
  • Frame End (= the camera is ready for a new trigger)
  • DeviceTemperatureStateNormal (= Mainboard temperature is between mvDeviceTemperatureLowerLimit and mvDeviceTemperatureUpperLimit)
  • DeviceTemperatureStateCritical (= Mainboard temperature is outside of mvDeviceTemperatureLowerLimit and mvDeviceTemperatureUpperLimit)
  • DeviceTemperatureStateOverTemperature (= Mainboard temperature exceeds maximum allowed temperature)

Setting Event notifications using ImpactControlCenter

To activate the notifications, just

  1. Select the Event via "Setting → Base → Camera → GenICam → Event Control → Event Selector", e.g. ExposureEnd .
  2. Set the "Event Notification" to "On" .

Afterwards, it is possible to attach a custom callback that gets called whenever the property is modified. E.g. if you want to attach a callback to the Frame ID after the exposure was finished, you have to

  1. select "Setting → Base → Camera → GenICam → Event Control → Event Exposure End Data → Event Exposure End Frame ID",
  2. right-click on the property, and
  3. click on "Attach Callback".

    Figure 1: ImpactControlCenter - "Attach Callback" to Event Exposure End Frame ID

Now, you can track the property modifications in the output window:

Figure 2: ImpactControlCenter - Output window with the Event notifications

You can find a detailed Callback code example in the C++ API manual.