Balluff - BVS CA-UB Technical Documentation
Loading...
Searching...
No Matches
NVIDIA Jetson™ AGX Orin

General

CPUArm Cortex-A78AE v8.2 @ 2.2GHz
Cores12
RAM32GB
USB2.0 Interfaces4
USB3.2 Interfaces3
Ethernet1x1 GbE + 1x10 GbE
PCIe2x8 + 1x4 + 2x1
Gen 4.0
Note
The above table describes the specification of the NVIDIA Jetson™ AGX Orin Developer Kit.
Note
The following tests were conducted on JetPack 5.1.2 with power mode MAXN.

Test Setup

Test setup

Additional Settings

Impact Acquire - System Settings

SettingValue
Request Count20
Note
A Request in the Impact Acquire API represents a buffer where an image with the current device configuration is captured into. In order to avoid losing images at a high FPS, it's recommended to increase the number of these request buffers (i.e. ' RequestCount' in ' SystemSettings', by default the value is set to 4 for Balluff USB2.0 cameras), so that the device driver can continue capturing image data even if the host application is sometimes slower at processing an image than the camera at transferring one. As a rule of thumb, the number of capture buffers should be configured roughly within the range of FPS/2 and FPS/5. In the following test, the RequestCount is set to 20 which is roughly FPS/5.

Benchmarks

CameraResolutionPixel FormatFrame Rate [Frames/s]Bandwidth [MB/s]CPU Load (without image display)
mvBlueFOX-ML/IGC200wG752 x 480Mono893.7133.88~4%
Note
: Camera models of type BVS CA-UB1* are recommended. The following problems might be observed when using the camera models of type mvBlueFOX-ML/IGC*:
  • On ARM platforms, there might be several lost frames at the beginning of acquisition start.
  • If the device has already been initialized, between acquisition stop and restart, there will be lost frames registered in the statistics, because the image sensor keeps generating image data also after the acquisition stop as long as it has been initialized.