Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
Saving User Settings In The Non-volatile Memory

Some cameras offer the possibility, to save up to 4 user sets in the camera's non-volatile memory directly. This means that all camera specific settings you've adjusted via ImpactControlCenter can be saved in a non-volatile memory.

Example: You have connected a flash via exposure out of the camera and you want to avoid an overload of the flash by maloperation, you can save a suitable shutter time, with which the camera will start.

To save your specific settings, set you properties in the "Setting → Camera → GenICam" section of ImpactControlCenter. Then, select in "User Set Control" your user set with the "User Set Selector", for example "UserSet1". Afterwards, save the user set with "int UserSetSave()". Finally, if you want that the camera starts with a specific user set (after power up), you have to select it with the "User Set Default Selector".

ImpactControlCenter - User set control
Attention
A firmware update will delete all saved register settings!