Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
GigE Vision™ Device Boot Behaviour

A GigE Vision™ compliant device can be configured to

  • use a persistent IP address (if supported by the device) and/or
  • use DHCP to obtain an IP address

Since the GigE Vision™ standard requires LLA to be enabled at all times the "Use LLA" control will never become modifiable.

Every GigE Vision™ compliant device must use the following IP protocol selection algorithm:

GigE Vision™ - IP protocol selection sequence

In the above image it can also be seen, why configuring both persistent and DHCP IP might be a valid setup: In case the persistent IP address for any reason has not been assigned successfully, a device could then still ask a DHCP server for a valid IPv4 address.