Impact Acquire SDK .NET
Loading...
Searching...
No Matches
GenICam

The mvGenTLConsumer library shipped as part Impact Acquire framework makes use of the GenICam™ reference implementation, which is hosted by the EVMA and can be downloaded from their website: http://www.emva.org. All license files belonging to the GenICam™ reference implementation are shipped with the libraries belonging to the GenICam runtime. They can be found in the licenses subdirectory of the GenICam™ reference implementation.

Used Versions

The following table lists which version of Impact Acquire does use which version of the GenICam reference implementation

Impact Acquire versionGenApi versionCPE name
since 1.10.501.1.1
since 1.10.741.1.2
since 1.10.952.0.0
since 1.11.02.0.1
since 1.11.422.1.1
since 1.12.532.3.0
since 2.7.02.4.0
since 2.15.03.0.0
since 2.16.13.0.1
since 2.28.03.1.0 (Jun 2018)
since 2.45.03.3.0 (Feb 2021)
since 2.50.03.4.1 (Jul 2023)
since 3.5.03.5.0 (Mar 17 2025)