Impact Acquire SDK .NET
Loading...
Searching...
No Matches
Non-MSI Based Setup Routines
Attention
Other setup routines should NOT include the driver files if this can be avoided, as this might cause version conflicts when the original installation package is installed as well and might also confuse the MSI engine when removing the original installation package, which might cause an incomplete package removal operation. However if this approach is desired this section provides a brief list of things that must be done of the target machine.
Note
Deprecated product families will NOT be described here!