At least four steps are necessary to capture a single image from a Balluff device. These steps are explained with the help of source examples from ImpactControlCenter.
Grants access to devices that can be operated by this software interface.
Definition DeviceManager.cs:157
static Device getDevice(int index)
Returns a pointer to a mv.impact.acquire.Device object.
Definition DeviceManager.cs:514
This class and its functions represent an actual device detected by this interface in the current sys...
Definition Device.cs:91
void open()
Opens a device.
Definition Device.cs:209
This namespace contains classes and functions belonging to the image acquisition module of this SDK.
Definition Enumerations.cs:2
Definition Enumerations.cs:2
Definition Enumerations.cs:2
A live acquisition (running inside a thread function) could be implemented as follows:
Thread thread = new Thread(delegate()
{
TDMR_ERROR result = TDMR_ERROR.DMR_NO_ERROR;
while ((result = (TDMR_ERROR)fi.imageRequestSingle()) == TDMR_ERROR.DMR_NO_ERROR) { };
if (result != TDMR_ERROR.DEV_NO_FREE_REQUEST_AVAILABLE)
{
Console.WriteLine("'FunctionInterface.imageRequestSingle' returned with an unexpected result: {0}({1})", result, ImpactAcquireException.getErrorCodeAsString(result));
}
if (pDev.acquisitionStartStopBehaviour.read() == TAcquisitionStartStopBehaviour.assbUser)
{
if ((result = (TDMR_ERROR)fi.acquisitionStart()) != TDMR_ERROR.DMR_NO_ERROR)
{
Console.WriteLine("'FunctionInterface.acquisitionStart' returned with an unexpected result: {0}({1})", result, ImpactAcquireException.getErrorCodeAsString(result));
}
}
Request pRequest = null;
int timeout_ms = 500;
int cnt = 0;
int requestNr = Device.INVALID_ID;
while (!terminated)
{
requestNr = fi.imageRequestWaitFor(timeout_ms);
pRequest = fi.isRequestNrValid(requestNr) ? fi.getRequest(requestNr) : null;
if (pRequest != null)
{
if (pRequest.isOK)
{
}
else
{
Console.WriteLine("Error: {0}", pRequest.requestResult.readS());
}
pRequest.unlock();
fi.imageRequestSingle();
}
else
{
Console.WriteLine("imageRequestWaitFor failed ({0}, {1}), timeout value too small?", requestNr, ImpactAcquireException.getErrorCodeAsString(requestNr));
}
}
{
if ((result = (TDMR_ERROR)fi.acquisitionStop()) !=
TDMR_ERROR.DMR_NO_ERROR)
{
Console.WriteLine("'FunctionInterface.acquisitionStop' returned with an unexpected result: {0}({1})", result, ImpactAcquireException.getErrorCodeAsString(result));
}
}
fi.imageRequestReset(0, 0);
});
TDMR_ERROR
Errors reported by the device manager.
Definition mvDriverBaseEnums.cs:2558
TAcquisitionStartStopBehaviour
Defines valid modes for acquisition start/stop behaviour.
Definition mvDriverBaseEnums.cs:76