Impact Acquire SDK Java
Loading...
Searching...
No Matches
Qt

Some example applications of Impact Acquire make use of the Qt (https://www.qt.io/) framework

Qt License

The Qt framework comes under various licenses beyond the scope of this document. The exact conditions an licenses can be obtained from the Qt Company.

Note
You might need to ship the source code using Qt and Impact Acquire unless you possess an appropriate Qt license! Get in touch with the Qt guys in case of doubt!

Used Versions

The binary versions of the applications shipped with Impact Acquire on Windows® have been built using Qt with following versions. The source code to these binaries is shipped as part of the SDK. Linux builds will not contain binaries but source code only. Applications will be compiled using the Qt version available on the target system.

Impact Acquire versionQt versionCPE name
since 2.30.15.5.0
since 2.50.05.15.9cpe:2.3:a:qt:qt:5.15.9:::::::*