|
Impact Acquire SDK Java
|
Triggering images can be realized by using the required device properties. Depending on the device type there might be different settings available which can be configured using the mvIMPACT.acquire.GenICam.AcquisitionControl class.
As trigger capabilities have a strong relationship to specific hardware it would be a good idea to check the corresponding translation dictionaries of the corresponding properties e.g.:
All trigger modes are defined by the enumeration
However, not every device will offer all these trigger modes but a subset of them. Valid trigger modes therefore can be found by reading the properties translation dictionary.
A sample on how to query a property's translation dictionary can be found here:
All trigger modes are defined by the enumeration
For more specified information about triggered images with CCD sensors, refer to the "More specific data" link in the sensor tables.