Impact Acquire SDK C++
Loading...
Searching...
No Matches
Used Third Party Software

This SDK and its underlying libraries and device drivers as well as some of the applications shipped with the Impact Acquire packages make use of a couple of third party software packages that come with various licenses. This section is meant to list all these packages and to give credit to those whose code helped in the creation of the Impact Acquire SDK.

Copies of the original license files that have been shipped with the third party packages will also be part of the installation when the third party software is also needed for using certain Impact Acquire features. The corresponding license file will be located in a sub-folder of the Toolkits folder of the installation directory.

A software bill of materials (SBOM) is also available on request. The SBOM is a machine-readable list of all third party software packages used in Impact Acquire and their corresponding licenses. It can be obtained by contacting the Impact Acquire support team. See Imprint for contact information.