Impact Acquire SDK C++
Loading...
Searching...
No Matches
.NET Standard Support

In case an application makes use of the Impact Acquire .NET Standard interface the corresponding libraries must be deployed on the target system as well. Were and what version of these libraries must be shipped is explained in the Building, Linking And Running Applications Using Impact Acquire chapter of the .NET API manual.

Depending on the used functionalities the following libraries are necessary:

  • mv.impact.acquire.dll (always needed)
  • mv.impact.acquire.examples.helper.dll (needed if features from this module have been used)
Attention
Even if the listed files have the same names as the ones for the .NET interface the files are NOT identical. Refer to chapter Locating Runtime Libraries to get some information where they are located in the default installation.