Impact Acquire SDK C
Loading...
Searching...
No Matches
Linux

Requirements

Additional packages will be needed to use all features of Impact Acquire.

Compiler etc. for building applications:

  • build-essential (meta package)
  • gcc 5.5.0 environment or newer
  • cmake 3.10 or newer

Additional packages (mandatory) for running applications:

  • OpenMP runtime

wxWidget release 3.0 or 3.2 packages, e.g.

  • libwxbase3.0-0v5
  • libwxbase3.0-dev
  • libwxgtk3.0-gtk3-0v5
  • libwxgtk3.0-gtk3-dev
  • libwxgtk-webview3.0-gtk3-0v5
  • libwxgtk-webview3.0-gtk3-dev
  • wx3.0-headers
  • libgtk2.0-dev
Note
The names of the packages mentioned above are Debian / Ubuntu specific. Other distributions (e.g. SuSE, Arch, Redhat, ...) will use different names.

The installation script will ask if the packages should be downloaded during the installation process. If some of the packages are not installed some features might not be available. If the e.g. wxWidgets related packages are missing on the target system then all GUI application coming as part of the Impact Acquire installation won't be available.

Installation

To use a (camera) device in Linux (capture images from it and change its settings), a software stack is needed, consisting of several libraries and several configuration files. These files are required during runtime.

To develop applications that can use the device, an API containing header files, makefiles, samples, and a few libraries is needed. These files are required at compile time.

Both file collections are distributed in a single package which is available in the Download section of the Balluff website. This package is distributed as a single installer script (e.g. ImpactAcquire-x86_64-linux-3.8.1.sh). The script contains everyhing needed to install ImpactAcquire.

The following table shows the supported platforms and the corresponding installation script name:

ArchitecturePackage
ARM64ImpactAcquire-arm64-linux-3.8.1.sh
ARMhfImpactAcquire-armhf-linux-3.8.1.sh
x86_64ImpactAcquire-x86_64-linux-3.8.1.sh

The following example explains the installation process for the x86_64 package. The installation process for other packages will work almost identically except that different names are used, as mentioned in the previous table.

  • Please start a console and change into the directory where the installation script is located e.g. /home/username/Downloads :
    cd /home/username/Downloads 
    Note
    If root permissions are needed, the script will ask for the permissions. There is no need to call it with root permissions.
  • You might need to enable the execute flag with:
    chmod a+x ImpactAcquire-x86_64-linux-3.8.1.sh
  • Run the install script:
    ./ImpactAcquire-x86_64-linux-3.8.1.sh

During installation, the script will ask if it should build all tools and samples.

Note
The installation script has been developed for Ubuntu/Debian, SUSE Linux and Red Hat Linux based distributions. On other distributions some features of the installation script may or may not work. Get in touch with us if you encounter any problems!

The installation script checks for package dependencies described above and installs them with the respective standard package manager (e.g. apt-get) if necessary. So an Internet connection is recommended.

Note
  • Nothing is written to the directory containing the script during execution, so no write access to the directory is needed in order to execute the script.
  • In case one or more of the packages the Impact Acquire framework depends on are not yet installed on your system, the script tries to install the missing packages. Therefore, when something is missing, Internet access is required during the installation.