Impact Acquire SDK C
Loading...
Searching...
No Matches
SWIG

The Java as well as the Python interface of Impact Acquire is generated with the help of SWIG (http://www.swig.org).

SWIG License

The source code of SWIG comes under a GPL license. The output generated using SWIG can use any license depending on the need of the user.

More details regarding licenses can be found on the SWIG homepage in the legal department section. At the time of writing this was http://www.swig.org/legal.html.

Used Versions

The following table lists which version of Impact Acquire was built with which version of SWIG.

Impact Acquire versionSWIG version
since 2.22.02.0.12 (Feb 9 2014)
since 2.33.03.0.12 (Jan 28 2017)
since 2.35.04.0.1 (Aug 21 2019)
since 3.1.04.2.0 (Dec 31 2023)
since 3.6.04.3.1 (Apr 15 2025)