Impact Acquire SDK C
Loading...
Searching...
No Matches
Log-file Support

If your application shall be able to generate log output one of following directories must be created on the target system:

Apart from that these files must be installed into this directory:

  • mvDebugFlags.mvd
  • logo.png
  • mvIMPACT_acquireLogFile.xsl
  • mvLogFileViewer.html
  • sarissa.js
  • Apache.txt (this must be shipped with mvLogFileViewer.html and sarissa.js for legal reasons as part of the file make use of code under the Apache 2.0 license)

The first file is discussed in detail in the Logging chapter of this manual, the latter files are only needed if the standard Balluff Impact Acquire log-file style shall be used(XML with stylesheet transformation). To find out how to embed your own log-file stylesheet please refer to the chapter about the logging mechanism. Here it also explained how to create plain XML log files and XML files that can be viewed using mvLogFileViewer.html.