Balluff - BVS CA-SF Technical Documentation
Loading...
Searching...
No Matches
What's inside and accessories

Due to the varying fields of application the BVS CA-SF devices are shipped without accessories. The package contents:

  • BVS CA-SF

For the first use of BVS CA-SF devices we recommend the following accessories to get the camera up and running:

  • a USB3 cable
  • a lens
Note
Although maximum cable length is not specified in the USB 3 standard, the electrical properties of the cable and signal quality limitations may define the practical maximum length. There are different USB 3 cable qualities available on the market. If you want to use your own USB 3 cables, you have to ensure that the data quality and shielding of the cable is sufficient. As a rule of thumb thin cables will only work for short distances up to max. 3m. Better cable qualities which go alongside with thicker cable diameter will allow longer distances such as 5m or even 8m. We recommend to use the cables we supply to be on the safe side.

Accessories for the BVS CA-SF

Recommended accessories for the BVS CA-SF can be found on the product pages: