|
Balluff - BVS CA-GX0 / BVS CA-GX2 Technical Documentation
|
Some sensors in the Pregius sensor family of the third and newer generations support a dual exposure mode, i.e. after a trigger event, for example, different image areas can be exposed to light at the same time differently.
To activate the dual exposure mode there is the exposure mode called mvMultiZone.
If this mode is selected you can set the mvExposureZoneHeight. This property represents the desired height of the upper zone (Zone0). The desired height is relative to the max sensor height. The step is the same as the property Height in ImageFormatControl. The value of mvExposureZoneHeight will be internally evaluated and approximated to the nearest real sensor upper zone height. For your convenience we introduced a read only property mvExposureZoneResultingHeight, which informs you the real sensor upper zone height.
The exposure time of the different zones can be specified using the ExposureTimeSelector. Possible zones are
To activate the dual exposure, just
#include <mvIMPACT_CPP/mvIMPACT_acquire_GenICam.h> // more code GenICam::AcquisitionControl ac( pDev ); ac.exposureMode.writeS( "mvMultiZone" ); // assuming max height is greater or equal 256 ac.mvExposureZoneHeight.write( 256 ); ac.exposureTimeSelector.writeS( "mvHorizontalZone0" ); ac.exposureTime.write( 150 ); ac.exposureTimeSelector.writeS( "mvHorizontalZone1" ); ac.exposureTime.write( 900 ); // Backward compatibility: // If you wish to keep using mvExposureHorizontalZoneDivider // you don't need to set mvExposureZoneHeight above. // It will be set internally to represent the value // of mvExposureHorizontalZoneDivider //ac.mvExposureHorizontalZoneDivider.write( 50 ); // more code