Balluff - BVS CA-GX0 / BVS CA-GX2 Technical Documentation
Loading...
Searching...
No Matches
Accessing log files

If you need support using our products, you can shorten response times by sending us your log files. Access to the log files varies depending on the operating system:

Windows

Since
Version 2.11.9 of Impact Acquire

You can access the log files in Windows® using ImpactControlCenter. The way to do this is described in "Accessing Log Files" in the "Impact Acquire SDK GUI Applications" manual.

Linux

Since
Version 2.24.0 of Impact Acquire

You can access the log files in Linux via /opt/ImpactAcquire/data/logs .

You can also extract the directory using the following command

env | grep MVIMPACT_ACQUIRE_DATA_DIR

or move into the directory directly via

cd $MVIMPACT_ACQUIRE_DATA_DIR/logs

For older versions:

Like on Windows®, log files will be generated, if the activation flag for logging called mvDebugFlags.mvd is available in the same folder as the application (however, using Windows® log files will be generated automatically, because the applications are started from the same folder). By default, on Linux the mvDebugFlags.mvd will be installed in the installation's destination folder in the sub-folder "apps". For example, if the destination folder was "/home/workspace", you can locate the mvDebugFlags.mvd like the following way:

user@linux-desktop:~$
// <- Starting the console window, you will be in the home directory: /home/
user@linux-desktop:~$ cd workspace/apps/
// <- Change the directory
user@linux-desktop:/home/workspace/apps$ ls -l
// <- List the directory
total 144
drwxr-xr-x  9 user user  4096 Mai 21 15:08 Callback
drwxr-xr-x  8 user user  4096 Mai 21 15:08 Callback_C
drwxr-xr-x  9 user user  4096 Mai 21 15:08 CaptureToUserMemory_C
drwxr-xr-x  3 user user  4096 Mai 21 15:03 Common
drwxr-xr-x 11 user user  4096 Mai 21 15:09 ContinuousCapture
drwxr-xr-x  9 user user  4096 Mai 21 15:09 ContinuousCaptureAllDevices
drwxr-xr-x  6 user user  4096 Mai 21 15:09 ContinuousCaptureFLTK
drwxr-xr-x  9 user user  4096 Mai 21 15:09 ContinuousCapture_C
drwxr-xr-x 11 user user  4096 Mai 21 15:09 DigitalIOs
drwxr-xr-x 11 user user  4096 Mai 21 15:09 GenericInterfaceLayout
drwxr-xr-x 11 user user  4096 Mai 21 15:09 GenICamInterfaceLayout
-rw-r--r--  1 user user   854 Mai 21 15:03 Makefile
-rw-r--r--  1 user user  7365 Mai 21 15:03 Makefile.samp.inc
-rw-r--r--  1 user user 20713 Mai 21 15:03 mvDebugFlags.mvd
// <- Log activation flag
drwxr-xr-x  7 user user  4096 Mai 21 15:09 DeviceConfigure
drwxr-xr-x  6 user user  4096 Mai 21 15:10 IPConfigure
drwxr-xr-x  6 user user  4096 Mai 21 15:11 ImpactControlCenter
drwxr-xr-x  9 user user  4096 Mai 21 15:11 SingleCapture
drwxr-xr-x  9 user user  4096 Mai 21 15:11 SingleCaptureStorage

For log file generation you have to execute your app from the folder where mvDebugFlags.mvd is located. E.g. if you want to start ImpactControlCenter:

user@linux-desktop:/home/workspace/apps$ ./ImpactControlCenter/x86_64/ImpactControlCenter
// <- Start the executable from the folder, where \b mvDebugFlags.mvd is located.

Another possibility would be, to copy the mvDebugFlags.mvd file to the folder of the executable:

user@linux-desktop:/home/workspace/apps$ cp mvDebugFlags.mvd ./ImpactControlCenter/x86_64/ImpactControlCenter
// <- Copy the log activation flag
user@linux-desktop:/home/workspace/apps$ cd ./ImpactControlCenter/x86_64/
// <- Change the directory
user@linux-desktop:/home/workspace/apps/ImpactControlCenter/x86_64/$ ./ImpactControlCenter
// <- Start the executable

Afterwards, several log files are generated which are listed in files.mvloglist. The log files have the file extension .mvlog. Please send these files to our support team.

macOS

Since
Version 2.50.0 of Impact Acquire

you can extract the directory using the following command if you have set the environment variable $MVIMPACT_ACQUIRE_DATA_DIR permanently

printenv | grep MVIMPACT_ACQUIRE_DATA_DIR

or move into the directory directly via

cd $MVIMPACT_ACQUIRE_DATA_DIR/logs