|
Impact Acquire SDK C++
|
The following situation has been encountered:
mvGenTL_Acquire*.msi packages and installing an older version (2.16.1 or smaller) no network connections are displayed in the "Network And Sharing Center" any moreipconfig will still list the network interfaces correctly with their IP address howeverThis problem may occur when one of the following conditions is true:
mvGenTL_Acquire*.msi package with version 2.17.0 on Windows Vista or newermvGenTL_Acquire*.msi package with version 2.16.1 or smaller on that very same system afterwardsGigEConfigure on that systemRemove Driver buttonpnputil -e and press ENTER (since newer versions of Windows 10 -e has been superseded by /enum-drivers)pnputil -f -d (since newer versions of Windows 10 -e has been superseded by /delete-driver) and the name of the INF file containing the following data (the number between oem and .inf may vary): Published name : oem36.inf Driver package provider : MATRIX VISION GmbH Class : Network Service Driver date and version : 06/28/2016 3.0.1.55
mvGigECapture.sys or mvGigECapture2.sys from %windir%/System32/drivers and/or %windir%/SysWOW64/drivers (actually here you should NEVER see an instance of the filter driver thus this is a 32-bit folder on a 64-bit system and 32-kernel code is not supported on 64-bit Windows thus a buggy installation was the cause of this!).GigEConfigure tool on that systemInstall Driver button