|
Impact Acquire SDK C++
|
The following situation has been encountered:
When working with a GigE Vision™ compliant device and the GigE Vision™ filter driver on a Windows system sporadic Bluescreens (BSOD) can be observed. This is especially true when network data is lost from time to time and
This problem may occur when one of the following conditions is true:
mvGenTL_Acquire*.msi package with version smaller than 2.50.0mvGenTL_Acquire*.msi package with version smaller than 2.50.0If possible install a mvGenTL_Acquire*.msi package with version 2.50.0 or higher.
If that is not an option see the sections below.
GigEConfigure tool on that systemRemove Driver buttonInstall Driver buttonAfterwards the LAG group should display the filter driver as being enabled while the individual network interfaces forming the group should not. This configuration works! When adding additional LAG groups on that system or when deleting and recreating this one repeat this sequence!
When a network analyzer is needed the only option without updating the driver is to temporarily disable the filter driver on the network interface that shall be analyzed.