|
Impact Acquire SDK C++
|
One of the following situations has been encountered:
mvGenTL_Acquire*.msi packages during the removal of the package a bluescreen occurs and the driver is still listed as installed when restarting the system.GigEConfigure causes a bluescreen and the driver is still listed as enabled by this application when restarting the system.This problem may occur when one of the following conditions is true:
mvGenTL_Acquire*.msi package with a version smaller than 2.6.2 on a Windows 8.1 systemmvGenTL_Acquire*.msi package with a version smaller than 2.6.2 on a Windows 8 system and then updated this system to Windows version 8.1mvGigECapture.sys from winDir%/system32/drivers mvGenTL_Acquire package to version 2.6.2 or newer