|
Impact Acquire SDK C++
|
When working with USB3 Vision™ compliant devices thus when having the mvGenTL_Acquire package installed on a Linux system OR when using the GenICam GenTL compliant producer mvGenTLProducer.cti (libmvGenTLProducer.so) on a Linux system together with a 3rd party software package (e.g. OpenCV) also using libusb under the hood the application either crashes or devices cannot be used.
This problem may occur when the following conditions are true:
mvGenTLProducer.cti This is caused by compatibility issues within libusb. As on a Linux system there cannot be mixed versions of a shared object dynamically loaded into the same process the library loaded first is used and therefore depending on the load order of the libraries various things can happen. In order to overcome this problem Impact Acquire can be told to favour the systems version of libusb by defining an environment variable MVIMPACT_ACQUIRE_FAVOUR_SYSTEMS_LIBUSB before instantiating the Impact Acquire device manager.